KEA128 FSL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KEA128 FSL

Jump to solution
3,256 Views
testbed
Contributor III

Hello,

Is there a FSL for the KEA128 Kinetis MCU ? I see that there is one "Quick Start Package v5" for this MCU which contains all the driver code an necessary files which is just basic code far from the FSL found in the FRDM-K64_NFCNCI_Example project.

I am not interested to use the QSP v5 package for the KEA128, hence if there is any FSL for KEA128 or one that is compatible with the KEA128 please let me know. Thanks...

0 Kudos
Reply
1 Solution
2,762 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi testbed,

    The driver you post from the FRDM-k64 is from the KSDK2.0, but now the KSDK still doesn't contain the KEA series.

    So, you should refer to the KEA according driver:

http://www.nxp.com/assets/downloads/data/en/device-drivers/SDK-DRIVER-FRDM-KEA-S32DS.zip 

  Another KEA driver is porting from the KE series by our FAE, you also can refer to it:

https://community.nxp.com/servlet/JiveServlet/download/575986-1-363361/KEA_Driver_Lib_V1.zip 

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
2,762 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi testbed,

  What the FSL you mean? Freescale?

 Quick Start Package v5 is the FSL code which contains all the basic driver for the customer's reference.

 Except the Quick Start Package code, there also have some TRK-KEA128 code:

http://www.nxp.com/products/software-and-tools/hardware-development-tools/startertrak-development-bo...

Under software->lab and test software.

These are the driver, for the detail application, customer need to do it by themselves.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,762 Views
testbed
Contributor III

Hi Kerry,

Thanks for the info. I already have these files. I was referring to the freescale platform / hal driver package whose screenshot i have shown below. This is not for the KEA128 but for the FRDM-K64 board with K64 MCU. Only a few modules from this can be used for KEA128. So, i was wondering if this similar package was already available for KEA128.

fsl.png

0 Kudos
Reply
2,763 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi testbed,

    The driver you post from the FRDM-k64 is from the KSDK2.0, but now the KSDK still doesn't contain the KEA series.

    So, you should refer to the KEA according driver:

http://www.nxp.com/assets/downloads/data/en/device-drivers/SDK-DRIVER-FRDM-KEA-S32DS.zip 

  Another KEA driver is porting from the KE series by our FAE, you also can refer to it:

https://community.nxp.com/servlet/JiveServlet/download/575986-1-363361/KEA_Driver_Lib_V1.zip 

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------