KE1xZ LPFLL frequency range question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE1xZ LPFLL frequency range question

1,685 Views
isaotakashima
Contributor IV

According to feature in the KE1xZ reference manual, LPFLL has below feature.

• Programmable multiplier for up to 4 different frequency ranges

But I found only the following two frequency ranges.

00 LPFLL is trimmed to 48 MHz
01 LPFLL is trimmed to 72 MHz

Does the LPFLL of KE1xZ have the remaining two frequency ranges except the above?

Please reply as soon as possible.

Best regards

Takashima

Labels (1)
0 Kudos
Reply
2 Replies

1,543 Views
jonson_chen
NXP Employee
NXP Employee

Hi Takashima,

KE1xZ LPFLL supports 2 trimmed frequency ranges, will update the LPFLL descriptions in RM.

0 Kudos
Reply

1,543 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Takashima,

Yes, I think you are right. Programmable multiplier for only 2 different frequency ranges. I'll report this problem to internal system.

Thanks!

Jing

0 Kudos
Reply