KE1xZ LPFLL frequency range question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KE1xZ LPFLL frequency range question

1,633 次查看
isaotakashima
Contributor IV

According to feature in the KE1xZ reference manual, LPFLL has below feature.

• Programmable multiplier for up to 4 different frequency ranges

But I found only the following two frequency ranges.

00 LPFLL is trimmed to 48 MHz
01 LPFLL is trimmed to 72 MHz

Does the LPFLL of KE1xZ have the remaining two frequency ranges except the above?

Please reply as soon as possible.

Best regards

Takashima

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,491 次查看
jonson_chen
NXP Employee
NXP Employee

Hi Takashima,

KE1xZ LPFLL supports 2 trimmed frequency ranges, will update the LPFLL descriptions in RM.

0 项奖励
回复

1,491 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Takashima,

Yes, I think you are right. Programmable multiplier for only 2 different frequency ranges. I'll report this problem to internal system.

Thanks!

Jing

0 项奖励
回复