KE18xF FlexNVM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KE18xF FlexNVM

1,723件の閲覧回数
chaitanyakumarb
Contributor II

Hi all, I wanted to understand if FlexNVM can be configured as data flash and can be programmed any data using ROM Boot loader?

ラベル(1)
1 返信

1,619件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

The KE18F has 64kB of FlexNVM. The FlexNVM block can be configured to be used as data flash memory, EEPROM backup flash memory, or a combination of both. You can find detailed information on how to use this and implement it in the application note AN5338.It is possible to to use the ROM bootloader as well. You can also find the information regarding the structures needed to initialize it properly as well as the commands in the following document:

MCU Bootloader Reference Manual

 

Please let me know if you have any further questions.

Have a great day!

Sabina