KE18F WDOG Clock Capability

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KE18F WDOG Clock Capability

ソリューションへジャンプ
2,392件の閲覧回数
sean_dvorscak
Contributor III

I was wondering what the max frequency is for the watchdog on the KE18F MCU.  The reference manual has a table to describe the timeout capabilities, and I am confused on the last row of the table on page 716.  It says 20MHz (from bus or external).  I have my bus clock running at 60MHz.  Are these values just examples?  Can I run the watchdog up to the bus clock frequency, or will it max out at 20MHz?

sean_dvorscak_0-1609875959817.png

 

0 件の賞賛
返信
1 解決策
2,381件の閲覧回数
nxf58904
NXP Employee
NXP Employee

Hi,

From the RM we know that watch dog's max clock=BUS_CLK

And I make a project , it shows ok.

I hope this help you.

nxf58904_0-1609921628108.png

nxf58904_1-1609921871931.png

 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,381件の閲覧回数
nxf58904
NXP Employee
NXP Employee

Hi,

From the RM we know that watch dog's max clock=BUS_CLK

And I make a project , it shows ok.

I hope this help you.

nxf58904_0-1609921628108.png

nxf58904_1-1609921871931.png

 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 件の賞賛
返信
2,377件の閲覧回数
sean_dvorscak
Contributor III

Thank you for clarifying that.

0 件の賞賛
返信