KE18 ADC hardware trigger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KE18 ADC hardware trigger

1,304 次查看
davidsherman
Senior Contributor I

I can't seem to get the ADC to trigger from the LPIT or the FTM using the TRGMUX.  The ADC works from software triggers.  I can confirm the LPIT is running and it is triggering events, but I can't get the ADC interrupt to happen on any of the channels.  I have the pseudocode example in the KE18 manual implemented, but nothing happens.

SIM->ADCOPT |= SIM_ADCOPT_ADC0TRGSEL(1) | SIM_ADCOPT_ADC0PRETRGSEL(1);

TRGMUX0->TRGCFG[TRGMUX_ADC0_INDEX] = TRGMUX_TRGCFG_SEL0(0x07); // use LPIT ch0 for trigger source

 ADC0->SC2 |= ADC_SC2_ADTRG(1);

What am I missing?  Unfortunately, the ADC chapter is confusing on the subject of pretriggers and triggers.  I'm just trying to get the ADC to trigger at a regular interval.

0 项奖励
回复
2 回复数

1,181 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, David,

I think your above code is correct, can you post your code here so that we can have a review and debug?

BR

Xiangjun Rong

0 项奖励
回复

1,181 次查看
davidsherman
Senior Contributor I

I found it, I missed the part in the LPIT where it has to be stopped to change the interval.  I was modifying something that did software triggers, but part of it calculates the acquisition interval and it stopped the LPIT when it tried to update the interval.  Seems to be working now.

0 项奖励
回复