KE16F Vs. KE18F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE16F Vs. KE18F

2,702 Views
JRIIS
NXP Employee
NXP Employee

Customer asking about the implication from a technical point of view if they change their design from the MKE16F to the MKE18F.

This should be the same die so it should be fine to use both as long at they compile to the actual version.

Could I kindly ask for validation on this please?

Thanks,

/Jakob

 

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,682 Views
JRIIS
NXP Employee
NXP Employee

Hi Jing,

I need to understand all deference in detailed, when you say main difference is memory size then you indicate that there is other deference. Could you please point those out?

Thanks,

/Jakob

0 Kudos
Reply

2,673 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

KE18F has 2 CAN while KE16F has 1 CAN.

That's all I think.

 

Regards,

Jing

0 Kudos
Reply

2,691 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Jakob,

Yes. Their main difference is memory size.

 

Regards,

Jing

0 Kudos
Reply