KE16 CAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,894件の閲覧回数
davidsherman
Senior Contributor I

This might be a silly question, but it's not very clear from the documentation.  The KE16 has one FlexCAN channel.  I'm assuming that means it only has the CAN0 channel, but I wanted to make sure it wasn't CAN1 since the reference manual covers KE18 as well, which has both channels.

0 件の賞賛
返信
1 解決策
3,868件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi davidsherman,

  Sorry for making your confusing, normally, if just one module, from number 0.

  So, to the KE16, it is CAN0.

You also can use the CFG tool to check it, you can find it contains CAN0:

kerryzhou_0-1617676696362.png

The CFG tool can be downloaded from this link:

www.nxp.com/mcuxpresso

Wish it helps you!

If you still have questions about it, please kindly let me know.

 

Best Regards,

kerry

 

元の投稿で解決策を見る

4 返答(返信)
3,880件の閲覧回数
davidsherman
Senior Contributor I

You did not answer my question.  I know the KE16 only has one CAN module.  My question is, which one?  It's kind of important to know if you're laying out a board, because the CAN0 and CAN1 don't use the same pins.  Does the KE16 have CAN0, or is it CAN1?

0 件の賞賛
返信
3,869件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi davidsherman,

  Sorry for making your confusing, normally, if just one module, from number 0.

  So, to the KE16, it is CAN0.

You also can use the CFG tool to check it, you can find it contains CAN0:

kerryzhou_0-1617676696362.png

The CFG tool can be downloaded from this link:

www.nxp.com/mcuxpresso

Wish it helps you!

If you still have questions about it, please kindly let me know.

 

Best Regards,

kerry

 

3,861件の閲覧回数
davidsherman
Senior Contributor I

Thank you, that was helpful.

0 件の賞賛
返信
3,886件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi davidsherman,

 Please feel free to ask the technical questions, you are always welcome!

  MKE16 series just contains one CAN module, but MKE18 has 2 CAN modules:

kerryzhou_0-1617339218910.png

 

Wish it helps you!

Best Regards,

Kerry

 

0 件の賞賛
返信