KE16 CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE16 CAN

Jump to solution
3,807 Views
davidsherman
Senior Contributor I

This might be a silly question, but it's not very clear from the documentation.  The KE16 has one FlexCAN channel.  I'm assuming that means it only has the CAN0 channel, but I wanted to make sure it wasn't CAN1 since the reference manual covers KE18 as well, which has both channels.

0 Kudos
Reply
1 Solution
3,781 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi davidsherman,

  Sorry for making your confusing, normally, if just one module, from number 0.

  So, to the KE16, it is CAN0.

You also can use the CFG tool to check it, you can find it contains CAN0:

kerryzhou_0-1617676696362.png

The CFG tool can be downloaded from this link:

www.nxp.com/mcuxpresso

Wish it helps you!

If you still have questions about it, please kindly let me know.

 

Best Regards,

kerry

 

View solution in original post

4 Replies
3,793 Views
davidsherman
Senior Contributor I

You did not answer my question.  I know the KE16 only has one CAN module.  My question is, which one?  It's kind of important to know if you're laying out a board, because the CAN0 and CAN1 don't use the same pins.  Does the KE16 have CAN0, or is it CAN1?

0 Kudos
Reply
3,782 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi davidsherman,

  Sorry for making your confusing, normally, if just one module, from number 0.

  So, to the KE16, it is CAN0.

You also can use the CFG tool to check it, you can find it contains CAN0:

kerryzhou_0-1617676696362.png

The CFG tool can be downloaded from this link:

www.nxp.com/mcuxpresso

Wish it helps you!

If you still have questions about it, please kindly let me know.

 

Best Regards,

kerry

 

3,774 Views
davidsherman
Senior Contributor I

Thank you, that was helpful.

0 Kudos
Reply
3,799 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi davidsherman,

 Please feel free to ask the technical questions, you are always welcome!

  MKE16 series just contains one CAN module, but MKE18 has 2 CAN modules:

kerryzhou_0-1617339218910.png

 

Wish it helps you!

Best Regards,

Kerry

 

0 Kudos
Reply