KE06 does not wakeup on MSCAN interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KE06 does not wakeup on MSCAN interrupt

跳至解决方案
2,260 次查看
newke06user
Contributor I

Hi,

I am using KE06 (MKE06Z128xxx4, FRDM eval board) and putting it in deep sleep using following piece of code -

{

     SCB->SCR |= 1<<2; // Enable deep sleep feature

     __asm ("WFI \n");     // Wait for interrupt

}

I looks going in sleep but if i send a J1939 packet to it, it doesn't wake-up.

Please let me know if i am missing something.

Thanks

Vikas

标签 (1)
0 项奖励
回复
1 解答
2,027 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi vikas shrivastava,

   Did you configure the bit in the wake-up interrupt note before you entering power down mode?

NOTE

This interrupt can only occur if the MSCAN was in sleep mode

(SLPRQ = 1 and SLPAK = 1) before entering power down

mode, the wake-up option is enabled (WUPE = 1), and the

wake-up interrupt is enabled (WUPIE = 1).

Please check it.

Regards

Jingjing

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,028 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi vikas shrivastava,

   Did you configure the bit in the wake-up interrupt note before you entering power down mode?

NOTE

This interrupt can only occur if the MSCAN was in sleep mode

(SLPRQ = 1 and SLPAK = 1) before entering power down

mode, the wake-up option is enabled (WUPE = 1), and the

wake-up interrupt is enabled (WUPIE = 1).

Please check it.

Regards

Jingjing

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,027 次查看
newke06user
Contributor I

Hi Jingjing,

Thanks for your reply.

Looks like it started working (waking up with CAN message), the only additional thing after setting SLPRQ, SLPAK, WUPE, WUPIE i had to put small delay.

For now after wakingup it is not accepting any CAN messages, i am observing it and let you know.

I have another observation - if i keep the STLink debugger plugged to evaluation board, it doesn't go to sleep. But if i unplug the STLink from board and then restart, it goes to sleep. Is it expected behaviour or i am missing something.



0 项奖励
回复