KE06 PTF5 initial value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE06 PTF5 initial value

1,183 Views
clchen
Contributor I

Hi,

I am using KE06 LQPF package, and configuring pin29/PTF5 to 0/low as initial value.

It seems pin29/PTF5 still keeps at 1/high when power up, and goes to 0/low after about 500ms.

How to configure/set the initial value of pin29/PTF5 to make sure it is 0/low when power up.

Labels (1)
0 Kudos
Reply
1 Reply

1,150 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi cl chen,

This pin is default as analog function.

If you want to make sure it is 0/low when power up, you may need to add external pull-down resistor on this GPIO.

PTF5.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply