KE 06 stop mode wake-up problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE 06 stop mode wake-up problem

2,394 Views
bobmke
Contributor II

I'm trying to use the RTC to wake up the KE06 uP from Stop Mode. It says the RTC alarm interrupt will start the AWIC which in turn triggers the clocks to start running The NVIC then takes over to service the interrupt. However, there is no alarm interrupt in the user guide, just the RTIF interrupt. I have the RTC_SC RTIF and RTIE bits both set.

In stop mode, the NVIC is in static state. The platform clock runs the AWIC, but the pllatform clock is stopped in stop mode. So how can you get the RTC to wake up the processor? I'm using the internal clock source and the FFL to run the uP.

Labels (1)
0 Kudos
Reply
3 Replies

2,174 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

the alarm interrupt is rtc interrupt. The primary function of the Asynchronous Wake-up Interrupt Controller (AWIC) is
to detect asynchronous wake-up events in stop modes and signal to clock control logic to resume system clocking. After clock restart, the NVIC observes the pending interrupt and performs the normal interrupt or event processing.

Regards

Jing

0 Kudos
Reply

2,173 Views
mjbcswitzerland
Specialist V

Hi Bob
 
The RTC in the KE06 can be used to 'periodically' wake the processor from STOP mode. It is really only a 16 but timer but, when using a slow clock and high clock divider, can allow quite long periods - of course the period setting can be modified each time to emulate it firing at a certain time in the future (although not necessarily with high precision).
You also need to ensure that the chosen clock source is operation in STOP mode.

Attached is a binary file for the FRDM-KE06Z board which shows time keeping implementation on the KE06 (on VCOM interface of OpenSDA at 115'200 Baud, go to the "admin" menu to find commands for setting time and date, viewing present time and setting alarms. The present low power operating mode can be requested with "show_lp" and changed using "set_lp")

Regards

Mark

 


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)
Kinetis: http://www.utasker.com/kinetis.html


Kinetis KE06
- http://www.utasker.com/kinetis/FRDM-KE06Z.html

Time-keeping
- http://www.utasker.com/docs/uTasker/uTasker_Time.pdf

KL RTC
- http://www.utasker.com/kinetis/KL_RTC.html

Low Power Wake-up
- http://www.utasker.com/kinetis/LLWU.html

0 Kudos
Reply

2,173 Views
bobmke
Contributor II

I think I may have figured it out.

One of the functions I call from my RTC interrupt routine runs longer than the interrupt time sometimes.

If the interrupt flag in the RTC status register is already set when I put the uP to sleep, will it fail to wake up?

0 Kudos
Reply