KDS debugger with DAPLink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS debugger with DAPLink

1,963 Views
roymessinger
Contributor V

I've just updated the bootloader and firmware to DAPLink (OpenSDA Serial and Debug Adapter|NXP )

How do I use the KDS debugger, when I connect the microUSB to the FRDM K64 board?

I don't see any OpenSDA in the KDS:

pastedImage_6.png

0 Kudos
Reply
3 Replies

1,681 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi roymessinger,

Please refer this "KDS Debug Configurations (OpenOCD, P&E, Segger)".
If you want to use OpenSDA, please select GDB PEMicro Interface Debugging.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,681 Views
roymessinger
Contributor V

Thanks, but not working. FRDM k64 is connected via USB (to host):

pastedImage_2.png

And I'm getting this error message:

pastedImage_3.png

0 Kudos
Reply

1,681 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I can see the OpenSDA port in PEMicro Interface Settings and Device Manager.

Debug Port OpenSDA.png
Have you try to use other firmware application?
See also the Note if you are using Windows 10.

OpenSDA firmware.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply