KDS debugger with DAPLink

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KDS debugger with DAPLink

1,381 次查看
roymessinger
Contributor V

I've just updated the bootloader and firmware to DAPLink (OpenSDA Serial and Debug Adapter|NXP )

How do I use the KDS debugger, when I connect the microUSB to the FRDM K64 board?

I don't see any OpenSDA in the KDS:

pastedImage_6.png

0 项奖励
回复
3 回复数

1,099 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi roymessinger,

Please refer this "KDS Debug Configurations (OpenOCD, P&E, Segger)".
If you want to use OpenSDA, please select GDB PEMicro Interface Debugging.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,099 次查看
roymessinger
Contributor V

Thanks, but not working. FRDM k64 is connected via USB (to host):

pastedImage_2.png

And I'm getting this error message:

pastedImage_3.png

0 项奖励
回复

1,099 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

I can see the OpenSDA port in PEMicro Interface Settings and Device Manager.

Debug Port OpenSDA.png
Have you try to use other firmware application?
See also the Note if you are using Windows 10.

OpenSDA firmware.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复