KDS debugger with DAPLink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS debugger with DAPLink

2,050件の閲覧回数
roymessinger
Contributor V

I've just updated the bootloader and firmware to DAPLink (OpenSDA Serial and Debug Adapter|NXP )

How do I use the KDS debugger, when I connect the microUSB to the FRDM K64 board?

I don't see any OpenSDA in the KDS:

pastedImage_6.png

0 件の賞賛
返信
3 返答(返信)

1,768件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi roymessinger,

Please refer this "KDS Debug Configurations (OpenOCD, P&E, Segger)".
If you want to use OpenSDA, please select GDB PEMicro Interface Debugging.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,768件の閲覧回数
roymessinger
Contributor V

Thanks, but not working. FRDM k64 is connected via USB (to host):

pastedImage_2.png

And I'm getting this error message:

pastedImage_3.png

0 件の賞賛
返信

1,768件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

I can see the OpenSDA port in PEMicro Interface Settings and Device Manager.

Debug Port OpenSDA.png
Have you try to use other firmware application?
See also the Note if you are using Windows 10.

OpenSDA firmware.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信