KBoot stuck in bootloader in Linux?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KBoot stuck in bootloader in Linux?

2,741件の閲覧回数
joeygouly
Contributor IV

Hi all,

I've been developing my project using KL27Z on OS X. Everything works fine.

Today I plugged my PCB via USB into my Linux machine and it doesn't work!

It connects and shows up in 'dmesg' as the Kinetis Bootloader.. however it never gets out of bootloader mode and into my application.

Anyone got any ideas?

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

2,560件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Joey,

I think I misunderstood your question and I feel sorry for that.

You can reconfigure the flash configuration filed through the approach.

https://community.nxp.com/message/347605

Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,560件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Joey,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

I was wondering if you can tell me what kind of the KBOOT version you use.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,560件の閲覧回数
joeygouly
Contributor IV

Hi,

It's version 1.2, my device returns 0x14B.

Thanks,

Joey

0 件の賞賛
返信

2,560件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Joey,

I'd highly recommend that you should choose the latest version —KBOOT V2.0 instead of the V1.2, as the the KBOOT V2.0 is verified on the Linux OS.

KBOOT:

Kinetis Bootloader|NXP

Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,560件の閲覧回数
joeygouly
Contributor IV

I'm talking about the ROM bootloader, that is on the MKL27Z. Assuming it's really ROM, I won't be able to upgrade!

Will new KL27Z chips come with kboot 2.0 in ROM?

I got around the issue now by changing by FOPT settings to not always boot to the bootloader.

Joey

0 件の賞賛
返信