KBI in KEA-128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KBI in KEA-128

1,551件の閲覧回数
vignesh_vb_7
Contributor IV

Hi,

     Is it possible to use 2 KBI pins in a single KBI module? will there be any problem if i use KBI having another peripheral pin ? 

2 返答(返信)

1,375件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi vignesh balaji,

   You can use 2 KBI pins in one KBI module,  but you should take care of this point in the reference manual:

44.jpg

    So, if when one KBI pin is in asserted state, then another KBI pin detect the edges in the same KBI module may be ignored, that's why I suggest you use two pin in different KBI module .

  

Wish it helps you!

If you still have question, please contact me!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------


1,375件の閲覧回数
vignesh_vb_7
Contributor IV

Thank you Jing,

                         I controlled 2 KBI pins in the same KBI module by flipping the polarity of edges inside the interrupt

0 件の賞賛
返信