K82: WDOG in Stop mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K82: WDOG in Stop mode

1,300 Views
EugeneHiihtaja
Senior Contributor I

Hi !

I have configured WDOG in way that it require update in Stop mode as well:

WDOG_GetDefaultConfig(&config);
config.prescaler = kWDOG_ClockPrescalerDivide1;
config.clockSource = kWDOG_LpoClockSource; // 1ms
config.workMode.enableWait = true; // If update in Wait is required
config.workMode.enableStop = true; // If update in LLS3 is required
config.timeoutValue = 5000; // ms
config.enableWdog = true;
WDOG_Init(WDOG, &config);

/* Accessing register by bus clock. */
for (uint32_t i = 0; i < 256U; i++)
{
(void) WDOG->RSTCNT;
}

It work fine when RTOS is running and stay under _WFI()

But in LLS3 mode it looks like as disabled and reset is not happens.

Should it cause reset in LLS3 mode if it not updated by WDOG_Refresh(WDOG) API ?

What is right way for update WDOG timeout on fly  ? What should be enabled/disabled or WDOG_Init() with new parameters is OK ?

Regards,

Eugene

0 Kudos
Reply
1 Reply

1,210 Views
jorge_a_vazquez
NXP Employee
NXP Employee

HI Eugene Hiihtaja 

WDOG is not enabled in LLSx power mode, in this mode watchdog is static, which mean that register are retained but the module is not enabled.

The option in the API function is for STOP mode, which is different ofLLS and where the module is working (from low power clocks).

Hope this helps

Best regards

Jorge Alcala

0 Kudos
Reply