K70 Nandflash programming with P&E Cyclone Fx?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K70 Nandflash programming with P&E Cyclone Fx?

跳至解决方案
2,106 次查看
arnogir
Senior Contributor II

Hello,

I post this question on P&E micro forum but without success since many month!

So I try here! :

I asked in the P&E micro forum if Nandflash algorithm is possible with Cyclone FX.

Somebody answer me NandFlash is not supported but I don't know if it is because no algorithm exist yet or if Cyclone Hardware is not designed for this?

Because Kinetis has a NandFlash Controler (NFC). It will be damaging that the Cyclone does not know how to do it! My post is here:

http://www.pemicro.com/forums/forum.cfm?forum_topic_id=5230&forum_id=7#c13556

Then NandFlash DataSheet is here: http://datasheet.octopart.com/MT29F2G08ABAEAWP%3AE-Micron-datasheet-11549997.pdf

And I attached the Scheme of the used board on my side (SQM4-K70) Manufacturer website:
http://www.sqm4.com/sqm4-k70-kinetis-module-eeprom

Then It is possible to have an algorithm which will be able with the Cyclone to Dump the External NandFlash Memory and write it?

Thank you

标签 (1)
0 项奖励
回复
1 解答
1,880 次查看
johnny_pe
Contributor III

Arnaud,

We currently do not support NAND Flash programming. All of our flash
programming capabilities only supports NOR flash programming. So we cannot support your Flash setup.

Regards,

Johnny

PEmicro

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,880 次查看
arnogir
Senior Contributor II

Hello

Nobody can help me about this?

0 项奖励
回复
1,880 次查看
arnogir
Senior Contributor II

Hello

It's been 9 months since I tried to get an answer to this question without success.
We have invested in the Cyclone in order to optimize our production.

Today we have several orders and a large volume to produce. I would like to have the answer to my question in order to prepare this production as well as possible.

Is somebody can help me?

0 项奖励
回复
1,881 次查看
johnny_pe
Contributor III

Arnaud,

We currently do not support NAND Flash programming. All of our flash
programming capabilities only supports NOR flash programming. So we cannot support your Flash setup.

Regards,

Johnny

PEmicro

0 项奖励
回复