K70 Nandflash programming with P&E Cyclone Fx?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K70 Nandflash programming with P&E Cyclone Fx?

Jump to solution
2,139 Views
arnogir
Senior Contributor II

Hello,

I post this question on P&E micro forum but without success since many month!

So I try here! :

I asked in the P&E micro forum if Nandflash algorithm is possible with Cyclone FX.

Somebody answer me NandFlash is not supported but I don't know if it is because no algorithm exist yet or if Cyclone Hardware is not designed for this?

Because Kinetis has a NandFlash Controler (NFC). It will be damaging that the Cyclone does not know how to do it! My post is here:

http://www.pemicro.com/forums/forum.cfm?forum_topic_id=5230&forum_id=7#c13556

Then NandFlash DataSheet is here: http://datasheet.octopart.com/MT29F2G08ABAEAWP%3AE-Micron-datasheet-11549997.pdf

And I attached the Scheme of the used board on my side (SQM4-K70) Manufacturer website:
http://www.sqm4.com/sqm4-k70-kinetis-module-eeprom

Then It is possible to have an algorithm which will be able with the Cyclone to Dump the External NandFlash Memory and write it?

Thank you

Labels (1)
0 Kudos
Reply
1 Solution
1,913 Views
johnny_pe
Contributor III

Arnaud,

We currently do not support NAND Flash programming. All of our flash
programming capabilities only supports NOR flash programming. So we cannot support your Flash setup.

Regards,

Johnny

PEmicro

View solution in original post

0 Kudos
Reply
3 Replies
1,913 Views
arnogir
Senior Contributor II

Hello

Nobody can help me about this?

0 Kudos
Reply
1,913 Views
arnogir
Senior Contributor II

Hello

It's been 9 months since I tried to get an answer to this question without success.
We have invested in the Cyclone in order to optimize our production.

Today we have several orders and a large volume to produce. I would like to have the answer to my question in order to prepare this production as well as possible.

Is somebody can help me?

0 Kudos
Reply
1,914 Views
johnny_pe
Contributor III

Arnaud,

We currently do not support NAND Flash programming. All of our flash
programming capabilities only supports NOR flash programming. So we cannot support your Flash setup.

Regards,

Johnny

PEmicro

0 Kudos
Reply