K70 Flexbus Problem - Bus Faults

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K70 Flexbus Problem - Bus Faults

3,624 次查看
crezyoz
Contributor IV

I have setup the Flexbus to read from a 16bit ADC. I am using AD0-AD15 and one chip select (CS1). I don't mind that it is multiplexed because I was thinking the RD line would just get the data at the correct part of the read cycle.

 

I am using Processor Expert.

 

I set the Flexbus up with a base address of ox60000000.

 

PE Automatically enables the clock to the FlexBus, or so it seems.

 

When I attempt to read with something like:

 

uint16Val = *((uint16 *)0x60000000)

or

uint32Val = *((uint32 *)0x60000000)

 

I get a bus fault. I can't figure out what I am doing wrong. Please Advise!!!

 

 

0 项奖励
回复
6 回复数

3,142 次查看
crezyoz
Contributor IV

update..

 

I found that the K70 Ref Manual depicts 0x90000000 as an external FlexBus memory area. Not 0x60000000 as the P.E. allows. Also, apparently 0xA0000000 is available as a slave device area.. not executable.

 

I checked the SIM registers and indeed the FlexBus is being clocked at 30Mhz and the clock gate is ON.

 

Still.. no matter what I do I can NOT acces the Flexbus address range without a Bus Fault.

 

Still in dire need of help on this. So frustrating that I can not get ANY repsonses to my posts here. I attempted to get a Freescale tech support person over the phone as well.  I may just have to switch to a different processor with better support. All three of my current projects were based on the K70 / K20 devices but this isn't funny.

 

 

0 项奖励
回复

3,142 次查看
J2MEJediMaster
Specialist I

Have you tried doing a search on this board using "flexbus"? There have been a number of threads covering Kinetic Flexbus issues.

 

---Tom

0 项奖励
回复

3,142 次查看
crezyoz
Contributor IV

ha! Yeah.. for 2 days. There isn't a single post on the internet regarding the FlexBus that mentions Bus Faults related to CS1. Not Anywhere. I think there is only ONE regarding the FlexBus and Processor Expert

 

Thanks though.. gave me a chuckle. ! Duh.

 

I still need an answer to this but I found that by clearing the bits in GROUP1's register of the FB_CSPMCR the fault would stop occuring .  Using the same base address and memory block for the other chip selects did NOT yield a bus fault then attempting to access the bus. That can't work though because it sets the multiplexing for CS1 to FB_ALE.

 

Would have been nice to get some help from Freescale on this one. But not a peep.

 

0 项奖励
回复

3,142 次查看
crezyoz
Contributor IV

UPDATE:

 

Freescale says you must have CS0 enabled no matter which other CSx you are using or you will get a bus fault. I couldn't find that documented. Perhaps you pros know that or understand it as a result of other parts of the architecture but it was a very helpful note from Freescale.

 

Still trying to determine, though, if I can attach a 16 bit device to the FlexBus and acquire 16 bit shorts with single reads form the device. THis is a 6 channel ADC which increments its internal buffer pointer with each _RD signal. I think the Flexbus is reading 16 bits as two bytes though I don't have BWEs enabled. Still working it.. 

 

thanks!

0 项奖励
回复

3,142 次查看
J2MEJediMaster
Specialist I
0 项奖励
回复

3,142 次查看
crezyoz
Contributor IV

Thanks! One of the firsts post I read 3 days ago. Not related to my problem.  That coder was using the wrong cast to access the port. I saw everything there is online. Everything.

0 项奖励
回复