K70 DMA transfers in DDR2 memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K70 DMA transfers in DDR2 memory

1,951件の閲覧回数
markdoxbeck
Contributor II

I am trying to understand the DMA settings needed to transfer 1,920,000 bytes from one section of DDR to another. I am working with D4D/eGui and need to utilize DMA transfers for the double buffering system. I am using MQX 4.0 and CW 10.6. The system is setup to use DMA channel 0. During this testing, no other DMA channels are active.

Caching has been DISABLED for memory region 7. This is needed to get any reasonable results.

Below are the DMA settings just prior to starting the DMA transfer. In order to get all the bytes (1,920,000), I need to set NBYTES_MLNO to a value of 960,000. I would have thought that either 1920000 would be used or 480,000 (=1920000/4) because I do have ATTR set to transfer 4 bytes at one time (SSIZE=2).

Can anyone explain why this value is needed?

PRE-DMA Settings
     DMA_ES: 0x00000000
   DMA_ERR: 0x00000000
     DMA_CR: 0x00000400
       SADDR: 0x70000000
          SOFF: 0x00000004
         SLAST: 0x00000000
       DADDR: 0x70400000
          DOFF: 0x00000004
         DLAST: 0x00000000
           ATTR: 0x00000202
       NBYTES: 0x000EA600 (DMA_TCD0_NBYTES_MLNO = 960000)
         CITER: 0x00000001
         BITER: 0x00000001
            CSR: 0x00000002

Attached is my ISR code. I found that I had to set the CSR to 0 in order to prevent multiple ISR calls from happening. The other statements in the ISR did not prevent this.

0 件の賞賛
返信
1 返信

1,920件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Sorry MQX 4.0 is too old, can you test it on MQX 4.2 

 

Unfortunately both are no longer supported and MQX 5 has cost

Regards Vicente

 

0 件の賞賛
返信