K70 DDR2 Write Read Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K70 DDR2 Write Read Problem

3,002 次查看
kayathrim
Fresh Out Contributor

Hi all,

We are using custom board K70 MCU. Problem in DDR2 write and read in some boards. I am using memory test program to test the DDR2. Configurations of DDR2 remains same as K70 Tower kit. I am shifting bit '1' 8 times at location 0x80000000 for databus test. While reading it 11111111 is not written properly, instead 00000000 is written. I have tested in various address also. How to solve this problem?

We are using DDR2 MT47H64M16HR-3IT:H

Regards,

Kayathri

标记 (3)
0 项奖励
回复
4 回复数

2,729 次查看
pbanta
Contributor IV

Hi,

Do you know if you can successfully write *any* value to 0x80000000?  Forget about shifting bits.  For example, can you write 0xA5A5A5A5 to 0x80000000 and read it back?

Paul

0 项奖励
回复

2,730 次查看
kayathrim
Fresh Out Contributor

Hi Paul,

I wrote 0xA5A5A5A5  at address 0x80000000. if i read back, I am getting 0x25 at location 0x80000000.

1.I have tried to write 0xA5A5A5A5 at entire DDR2 memory location. if i read back, 0x80000000= 0x25 and 0x80000001 = 0xA5.  I have attached screenshot of the memory herewith.

ddr2-memory.JPG

2. At address 0x80000001 if i write value from 00 to FF and read back value is ok.

3. At address 0x80000000 if i write value from 00 to FF and read back upto 7F is ok. For 0x80 to FF value, it is reading 00 to 7F again.

Regards,

Kayathri

0 项奖励
回复

2,730 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Kayathri

if you have some boards that works properly and in other the same software is having problem, this locks like there is a hardware issue on those boards

Please check if there is not some missing  capacitor o component, please also check the lines for the DDR comunication,or maybe if the K70 is properly solder to the PCB

Regards

Vicente

0 项奖励
回复

2,730 次查看
kayathrim
Fresh Out Contributor

Hi Vicente,

We have re-soldered the DDR and K70 doubting that the hardware may have the problems but still the problem continues.

Regards,

Kayathri

0 项奖励
回复