K70 ADC hardware average function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K70 ADC hardware average function

Jump to solution
3,180 Views
hemanthkumarven
Contributor II

All,

In the K70 Reference Manual, under section 39, 16-bit ADC it has been mentioned that hardware average function is supported.

In the K70 Datasheet document, (Doc. Name: K70P256M120SF3) under table -29 it is mentioned that no ADC hardware averaging function.

Is the hardware averaging function present as part of 16-bit ADC?

Thanks

Hemanth

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,607 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

Yes, hardware averaging is supported by ADC in K70. I think you refer to the next part of the datasheet right?

ADC.png

The "No ADC hardware averaging" just represents a condition. It means that a Crate between 37.037 and 461.467 Ksps can be achieved using continuous conversions and *without* enabling hardware averaging, but it does not mean that averaging is not supported.

I hope this clarifies.

Regards!,

Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,608 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

Yes, hardware averaging is supported by ADC in K70. I think you refer to the next part of the datasheet right?

ADC.png

The "No ADC hardware averaging" just represents a condition. It means that a Crate between 37.037 and 461.467 Ksps can be achieved using continuous conversions and *without* enabling hardware averaging, but it does not mean that averaging is not supported.

I hope this clarifies.

Regards!,

Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,607 Views
hemanthkumarven
Contributor II

Thanks for the Quick Reply Jorge..

Really appreciated..

Hemanth

0 Kudos
Reply