K66F Codec DA7212 Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K66F Codec DA7212 Configuration

1,305件の閲覧回数
haozh
Contributor I

Hello ,

I have two questions regarding the configuration of DA7212.

1. In the schematics, there are only one digital MIC connected to the MIC1, and MIC2 is floating. During the configuration of DA7212, it seems both MIC was enabled.Can you explain why?

2. The digital MIC AKU242 was configured as the right channel, so only the rising edge of the clock has right data. The falling edge doesn't have the data.  However, the configuration of DA7212 took the data from both edges(DMIC_DATA_SE L=1). Can you explain why?

Hao

pastedImage_2.png

/* DA7212_Input_MIC1_Dig */
{
{DIALOG7212_MICBIAS_CTRL, 0xA9},
{DIALOG7212_CP_CTRL, 0xF1},
{DIALOG7212_MIXIN_L_SELECT, 0x80},
{DIALOG7212_MIXIN_R_SELECT, 0x80},
{DIALOG7212_SYSTEM_MODES_INPUT, 0xFE},
{DIALOG7212_SYSTEM_MODES_OUTPUT, 0xF7},
{DIALOG7212_MIC_CONFIG, 0x07},
{DIALOG7212_MIC_2_GAIN, 0x04},
{DIALOG7212_MIC_2_CTRL, 0x84},
{DIALOG7212_MIC_1_GAIN, 0x01},
{DIALOG7212_MIC_1_CTRL, 0x80},
{DIALOG7212_ADC_FILTERS1, 0x08},
},

pastedImage_1.png

0 件の賞賛
返信
1 返信

1,222件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

The thread was resolved internally.

Best Regards,

Alexis Andalon

0 件の賞賛
返信