K66 connecting SDRAM with 32bit data path

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K66 connecting SDRAM with 32bit data path

1,323件の閲覧回数
unknowncoder
Contributor III

I want to connect a SDRAM with a 32bit data path to the K66?

The user guide specifies that the K66 supports 32bit data path. But I noticed that the SDRAM data pins only support 16 bit data path. 

Is it possible to use the Flexbus to compensate for the additional 16 data pins that are missing? If so how do I do this?

There is nothing in the user guide that specifies how to use a 32bit data path. Is it possible the user guide has mistakes?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,186件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi unknowncoder

K66 only supports 8-bit, 16-bit wide SDRAM blocks, not support 32-bit .

Regards

Daniel.

0 件の賞賛
返信