K66 connecting SDRAM with 32bit data path

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K66 connecting SDRAM with 32bit data path

1,369 Views
unknowncoder
Contributor III

I want to connect a SDRAM with a 32bit data path to the K66?

The user guide specifies that the K66 supports 32bit data path. But I noticed that the SDRAM data pins only support 16 bit data path. 

Is it possible to use the Flexbus to compensate for the additional 16 data pins that are missing? If so how do I do this?

There is nothing in the user guide that specifies how to use a 32bit data path. Is it possible the user guide has mistakes?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,232 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi unknowncoder

K66 only supports 8-bit, 16-bit wide SDRAM blocks, not support 32-bit .

Regards

Daniel.

0 Kudos
Reply