K66 : Legacy receive buffer descriptor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K66 : Legacy receive buffer descriptor

跳至解决方案
1,281 次查看
koichisakagami
Contributor II

Dear community,
We are checking a Legacy receive buffer descriptor.

In the manual K66P144M180SF5RMV2 Rev. 2, Table 50-33. Receive buffer descriptor field definitions
it is described that the Field "L" indicates the  "Last in frame".
       0 : The buffer is not the last in a frame.
       1 : The buffer is the last in a frame.

[Question]
       How do I recognize the first in a frame ?

Best Regards,
  Koichi Sakagami

标签 (1)
0 项奖励
回复
1 解答
1,160 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Koichi,

I think the L flag is a IPv4 specific flag, the "Flags/Fragment offset" data in IP layer can determine the L bit in RxBD.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,161 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Koichi,

I think the L flag is a IPv4 specific flag, the "Flags/Fragment offset" data in IP layer can determine the L bit in RxBD.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 项奖励
回复