K64F only enter Bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K64F only enter Bootloader

5,024 Views
chenlucas
Contributor I

Hello everyone,

I have a question about FRDM K64F board.

Today, I used K64F plugin computer 

But K64F OpenSDA Green LED isn`t bright work, if i press reset switch.

My computer will get K64F enter bootloader mode.(Green LED will blink)

My computer OS is windows 10, and I updated below firmware version.

OpenSDA version / bootloader

Thanks,

Tags (1)
0 Kudos
Reply
5 Replies

3,573 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Chen,

- There are three debug inter faces we can choose for OpenSDA: Segger J-Link OpenSDA, P&E OpenSDA interface, or Mbed interface.  

Please  Drag'n drop or copy and paste the corresponding  OpenSDA Application binary file into the BOOTLOADER drive from your computer file explorer.

About the detail steps please refer to :

OpenSDA Serial and Debug Adapter|NXP      

- Also there is a  summary for debug interface, it is for FRDM-K22, while it is the same with FRDM-K64 .

Summary of FRDM-K22F debug interface

Hope it helps!

 


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,573 Views
chenlucas
Contributor I

Hi Alice_Yang, 

Thank you,

I have follow the step update firmware K64F will reset.

But always enter bootloader.

I do not use K64F a period of time.

Final, K64F can normal work.

I don`t know the issue source.

but I have twice experience, I want to know the source.

I want to avoid the issue.

0 Kudos
Reply

3,573 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Chen,

How about on Win7 ?

And could you please take a video or screenshots about your steps .

BR

Alice

0 Kudos
Reply

3,573 Views
chenlucas
Contributor I

Hi Alice ,

My computer used win 10 OS.

Now, My K64F can get normal mode.

 My step is ...

step 1) Download SDA firmware 

step 2) Hold the reset sw

step 3) next plugin usb cable in computer 

step 4) disk appear bootloader disk in my computer

step 5) moving *.bin file to bootloader disk

Final K64F reset 

But firmware don`t update.

Thank Alice!

0 Kudos
Reply

3,573 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi,

1. I recommend you use another PC (it's better Win7) to check whether your board work well,

check the problem is your board or PC.

2. step 5) moving *.bin file to bootloader disk , please send this .bin file to me , I test it on my board.

BR

ALice

0 Kudos
Reply