K64F maxclock input source for ADC16 and ADHSC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K64F maxclock input source for ADC16 and ADHSC

1,682件の閲覧回数
ffonck
Contributor II

I've been trying to achieve max clock input for the ADC16 in a MK64FX512Vxx12. According to datasheet K64F Sub-Family Data Sheet this value shouldn't be higher than 18Mhz and ADHSC (High speed conversion) must be set for high frequency clocks:

asdqsdqd.pngasdqsdqd.png

But, https://www.nxp.com/pages/adc-calculator:ADC_CALCULATOR on the "instructions" section says:

índice.jpgíndice.jpg

So, can I clear ADHSC to maximize sample rate in spite of performance, or is it mandatory to used ADHSC at maximum clock frequency?

If it is mandatory, above what frequency does ADHSC need to be set?

 

0 件の賞賛
返信
1 返信

1,650件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi ffonck,

Yes, if you don't care about convert accuracy, you can set this bit to zero. The additional 2 clock is used by ADC internal comparator circuit for auto-zero. It allow enough settling time when the ADC clock is fast. Without this 2 clock, previous ADC sampling channel may interfere current channel.

 

Regards,

Jing 

0 件の賞賛
返信