K64F FTM capabilities?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K64F FTM capabilities?

ソリューションへジャンプ
2,595件の閲覧回数
davenadler
Senior Contributor II

Where are implemented FTM capabilities documented?
In Kinetis K64F Sub-Family Data Sheet it lists 4 FTM:
• Two 8-channel Flex-Timers (PWM/Motor control)
• Two 2-channel FlexTimers (PWM/Quad decoder)

Which FTM have what capabilities?
Do all FTM have quadrature decoder?
I can't seem to find this in the documentation...

Thanks!
Best Regards, Dave

ラベル(2)
0 件の賞賛
返信
1 解決策
2,549件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Dave,

 

Not all of the FTMs have quadrature decoders.

The two 2-channel FTMs (FTM1 and FTM2) each have a quadrature decoder.

The two 8-channel FTMs (FTM0 and FTM3) each have a 3-phase motor and 2 general purpose or stepper motors.

 

In case you need any more information on the K64F, I think the K64 Sub-Family Reference Manual is the document you were missing. You mentioned the data sheet but not the reference manual in your post so I wanted to make sure you had access to both.

 

Here is the link to the K64F on the NXP website:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

 

At the bottom of the page there is a section with all of the documentation for this device. The document I used to answer your question was the “Kinetis K64: 120MHz Cortex-M4F up to 1MB Flash 100-144pin” under reference manuals. Specifically, page 137.

 

Thank you for your question!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,550件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Dave,

 

Not all of the FTMs have quadrature decoders.

The two 2-channel FTMs (FTM1 and FTM2) each have a quadrature decoder.

The two 8-channel FTMs (FTM0 and FTM3) each have a 3-phase motor and 2 general purpose or stepper motors.

 

In case you need any more information on the K64F, I think the K64 Sub-Family Reference Manual is the document you were missing. You mentioned the data sheet but not the reference manual in your post so I wanted to make sure you had access to both.

 

Here is the link to the K64F on the NXP website:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

 

At the bottom of the page there is a section with all of the documentation for this device. The document I used to answer your question was the “Kinetis K64: 120MHz Cortex-M4F up to 1MB Flash 100-144pin” under reference manuals. Specifically, page 137.

 

Thank you for your question!

0 件の賞賛
返信
2,541件の閲覧回数
davenadler
Senior Contributor II

Thanks @vicentegomez, all set.

0 件の賞賛
返信