K64F: ADC 16 bits range

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K64F: ADC 16 bits range

1,176件の閲覧回数
cesarhoyos
Contributor I

Hello there,

I am working with development platform of K64F and I am programming the actions of the ADC for conversion in 16bits, single-ended working.

I have read the reference manual, but I am still not sure if I am right about range.

tablaTensionesADC.png

Following this, I have assumed that the input voltage range is between 0V and 3'6V.

Could anyone confirm this assumption?

Thanks for your attention,

0 件の賞賛
返信
1 返信

1,044件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Cesar Hoyos

It depends in your VDD, VDDA, VSS, VSSA and VREF voltages. For example if you supply VDD with 3.3V, VDDA must be 3.3V (+/- 0.1V) and then VREFH could be up to 3.3V, so your range is between VREFL and 3.3V.

Hope this help you.

Best Regards

Jorge Alcala

0 件の賞賛
返信