K64F: ADC 16 bits range

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K64F: ADC 16 bits range

1,160 Views
cesarhoyos
Contributor I

Hello there,

I am working with development platform of K64F and I am programming the actions of the ADC for conversion in 16bits, single-ended working.

I have read the reference manual, but I am still not sure if I am right about range.

tablaTensionesADC.png

Following this, I have assumed that the input voltage range is between 0V and 3'6V.

Could anyone confirm this assumption?

Thanks for your attention,

0 Kudos
Reply
1 Reply

1,028 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Cesar Hoyos

It depends in your VDD, VDDA, VSS, VSSA and VREF voltages. For example if you supply VDD with 3.3V, VDDA must be 3.3V (+/- 0.1V) and then VREFH could be up to 3.3V, so your range is between VREFL and 3.3V.

Hope this help you.

Best Regards

Jorge Alcala

0 Kudos
Reply