K64 SDHC interface with emmc device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K64 SDHC interface with emmc device

3,112件の閲覧回数
JHinkle
Senior Contributor I

The K64's SDHC states that it is compliant with MMC System Specification 4.2/4.3

I am looking into interfacing the K64's SDHC with a emmc device meeting specification 5.1.

I would like to use the 8 bit data interface.

I have not been able to find any information as to interfacing a 5.1 device with a 4.3 version controller.

Can this be done? 

What are the pro/cons associated with an "old" SDHC controller mating with the latest emmc devices.

Thanks in advance for any replies.

Joe

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,853件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Joe,

First of all, sorry for the later reply.

Could you check the eMMC card manufacturer specifications to see if the card is backwards compatible with previous versions?

Thanks for the attention.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,853件の閲覧回数
JHinkle
Senior Contributor I

Hi Mike:

Trying to get an App Engineer from Western Digital to answer a question is impossible.

I found an NXP i.MX6 mcu that had a similar question asked and the post stated that the SDK driver needed to be changed but it could be used (the NXP mcu supported 4.4 when the K64 supports specifications 4.2/4.3)

https://community.nxp.com/docs/DOC-332187

I was hoping to get some assurance that the K64 will perform properly before I go to the effort and expense of turning a new board to test it.

I do not believe there will be an issue of sector read or write. 

I was hoping the K64 supported the "trim" and "Bad Sector Management" capabilities associated with the emmc device. 

Do you know if that is possible?

Thanks.

Joe

0 件の賞賛
返信

2,853件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Joe,

I don't find K64 SDHC module support "trim" and "Bad Sector Management" capabilities.

I think K64 couldn't support those features.

best regards,

Mike

0 件の賞賛
返信