K64 RAMCode error while programming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K64 RAMCode error while programming

1,448 次查看
arvind_kumar08
Contributor I

K 64 RAMCode Error while programming

Hello

in one of our application we are using k64 Microcontroller. we are using Segger J link debugger for programming flash using Jtag.

when i am programming the micro flash with a .bin  file, the error message received is "failed to read back RAMCode for programming"

previously i was able to program the same micro multiple times.

please suggest the probable reason and solutions

arvind

标签 (1)
0 项奖励
回复
1 回复

1,358 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Arvind kumar,

    Do you also try the official K64 code, whether you can download that code, take an example, KSDK2.2-FRDM-K64F120M?

  You can download it from this link:

Welcome to MCUXpresso | MCUXpresso Config Tools 

SDK builder, select the K64 board, generate the code and download it.

  Please try the official code at first, if official code don't have the problem, it means your own project have the problem.

 Then you can give me some error picture on your side.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复