K64 RAMCode error while programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K64 RAMCode error while programming

1,332件の閲覧回数
arvind_kumar08
Contributor I

K 64 RAMCode Error while programming

Hello

in one of our application we are using k64 Microcontroller. we are using Segger J link debugger for programming flash using Jtag.

when i am programming the micro flash with a .bin  file, the error message received is "failed to read back RAMCode for programming"

previously i was able to program the same micro multiple times.

please suggest the probable reason and solutions

arvind

ラベル(1)
0 件の賞賛
返信
1 返信

1,242件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Arvind kumar,

    Do you also try the official K64 code, whether you can download that code, take an example, KSDK2.2-FRDM-K64F120M?

  You can download it from this link:

Welcome to MCUXpresso | MCUXpresso Config Tools 

SDK builder, select the K64 board, generate the code and download it.

  Please try the official code at first, if official code don't have the problem, it means your own project have the problem.

 Then you can give me some error picture on your side.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信