K64 RAMCode error while programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K64 RAMCode error while programming

1,365 Views
arvind_kumar08
Contributor I

K 64 RAMCode Error while programming

Hello

in one of our application we are using k64 Microcontroller. we are using Segger J link debugger for programming flash using Jtag.

when i am programming the micro flash with a .bin  file, the error message received is "failed to read back RAMCode for programming"

previously i was able to program the same micro multiple times.

please suggest the probable reason and solutions

arvind

Labels (1)
0 Kudos
Reply
1 Reply

1,275 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Arvind kumar,

    Do you also try the official K64 code, whether you can download that code, take an example, KSDK2.2-FRDM-K64F120M?

  You can download it from this link:

Welcome to MCUXpresso | MCUXpresso Config Tools 

SDK builder, select the K64 board, generate the code and download it.

  Please try the official code at first, if official code don't have the problem, it means your own project have the problem.

 Then you can give me some error picture on your side.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply