K64 Output Pulse Clarification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K64 Output Pulse Clarification

ソリューションへジャンプ
1,764件の閲覧回数
azurin
Contributor I

We would like to simulate a driver output using one of the K64 channels. Which will require us to do an initial pulse for, let’s say, 300ms and then output a PWM signal with a 5KHz frequency (50% duty cycle).

Do I need to use a specific output or will any will work?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,672件の閲覧回数
mjbcswitzerland
Specialist V

Hi Dana

The FlexTimers can be used to generate Frequencies/PWM signals and therefore I would recommend choosing a pin with FlexTimer output functionality.

That means one wit a pin multiplexer function of the type "FTMx_CHy"

Regards

Mark

http://www.utasker.com/kinetis.html

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,673件の閲覧回数
mjbcswitzerland
Specialist V

Hi Dana

The FlexTimers can be used to generate Frequencies/PWM signals and therefore I would recommend choosing a pin with FlexTimer output functionality.

That means one wit a pin multiplexer function of the type "FTMx_CHy"

Regards

Mark

http://www.utasker.com/kinetis.html

0 件の賞賛
返信