K64 Output Pulse Clarification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K64 Output Pulse Clarification

Jump to solution
1,765 Views
azurin
Contributor I

We would like to simulate a driver output using one of the K64 channels. Which will require us to do an initial pulse for, let’s say, 300ms and then output a PWM signal with a 5KHz frequency (50% duty cycle).

Do I need to use a specific output or will any will work?

Labels (1)
0 Kudos
Reply
1 Solution
1,673 Views
mjbcswitzerland
Specialist V

Hi Dana

The FlexTimers can be used to generate Frequencies/PWM signals and therefore I would recommend choosing a pin with FlexTimer output functionality.

That means one wit a pin multiplexer function of the type "FTMx_CHy"

Regards

Mark

http://www.utasker.com/kinetis.html

View solution in original post

0 Kudos
Reply
1 Reply
1,674 Views
mjbcswitzerland
Specialist V

Hi Dana

The FlexTimers can be used to generate Frequencies/PWM signals and therefore I would recommend choosing a pin with FlexTimer output functionality.

That means one wit a pin multiplexer function of the type "FTMx_CHy"

Regards

Mark

http://www.utasker.com/kinetis.html

0 Kudos
Reply