K61 FLEXCAN has no DMA support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K61 FLEXCAN has no DMA support

ソリューションへジャンプ
2,260件の閲覧回数
benjaminschroed
Contributor III

I've been looking at the Kinetis K series processors, and it appears the CAN interface (FLEXCAN) has no DMA support, only interrupt.  Is this correct, or is there a workaround to be able to utilize DMA, specifically for Rx?

Thanks.

タグ(2)
0 件の賞賛
返信
1 解決策
2,029件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Yes, you are correct. For Kinetis K61, FlexCAN is not a DMA request source and there has no way to use like that.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,030件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Yes, you are correct. For Kinetis K61, FlexCAN is not a DMA request source and there has no way to use like that.

0 件の賞賛
返信
2,029件の閲覧回数
benjaminschroed
Contributor III

Thank you for the confirmation.

0 件の賞賛
返信