K61 FLEXCAN has no DMA support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K61 FLEXCAN has no DMA support

跳至解决方案
2,306 次查看
benjaminschroed
Contributor III

I've been looking at the Kinetis K series processors, and it appears the CAN interface (FLEXCAN) has no DMA support, only interrupt.  Is this correct, or is there a workaround to be able to utilize DMA, specifically for Rx?

Thanks.

标记 (2)
0 项奖励
回复
1 解答
2,075 次查看
miduo
NXP Employee
NXP Employee

Hi,

Yes, you are correct. For Kinetis K61, FlexCAN is not a DMA request source and there has no way to use like that.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,076 次查看
miduo
NXP Employee
NXP Employee

Hi,

Yes, you are correct. For Kinetis K61, FlexCAN is not a DMA request source and there has no way to use like that.

0 项奖励
回复
2,075 次查看
benjaminschroed
Contributor III

Thank you for the confirmation.

0 项奖励
回复