K60F120M (120MHz) controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60F120M (120MHz) controller

1,231 Views
pet
Contributor I

I'm using K60F120M (120MHz) controller, a sram device is connected to the spi1 interface. I use the spi driver example code to access to the sram via dma. But I don't see at all a clock or data on the pins.

Has somebody tried the spi driver?

What could be the reason for that?

regards

Labels (1)
0 Kudos
Reply
1 Reply

1,084 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Please refer Kinetis 120MHz example code with below link, which provides DSPI example code.

KINETIS_120MHZ_SC  (Kinetis 120MHz bare metal sample code) :

TWR-K70F120M: Kinetis K70 120 MHz Tower System Module

Wish it helps.

0 Kudos
Reply