K60D100M - USB Device - Printer class code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60D100M - USB Device - Printer class code

2,427件の閲覧回数
swaminathanrath
NXP Employee
NXP Employee

Hi,

I am using TWR-K60D100M Tower Board with TWR-Serial and using the printer class example code from  Freescale USB Stackv 4.1.1; I could enumerate as Printer class and installed the Generic printer and when i start to print the Text document I could not get any data in USB_APP Call back function. Can you please help me on this?

Thanks & Regards,

Swaminathan.R

0 件の賞賛
返信
3 返答(返信)

2,163件の閲覧回数
cutworth
NXP Employee
NXP Employee

Hi,

Are you running the demo on WinXP or Win7? Did you follow the instructions in "Freescale USB device stack user guide" to install the USB driver? I found some problem when manually install USB driver for printer class demo on Win7.

Only after you have installed the driver, will the device listed in "Printer and Fax" lists.

So when you print a document, did you choose the printing device associated with printer class demo?

0 件の賞賛
返信

2,163件の閲覧回数
swaminathanrath
NXP Employee
NXP Employee

Hi,

I am using Win7, I had followed the steps which is provided in the "Freescale USB Device stack user guide.

I had chosen the Generic printer as mentioned in the document. Whether you could receive the data in the source code in EPOUT when you are trying to print the Text file?

Thanks & Regards,

Swaminathan.R

0 件の賞賛
返信

2,163件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

I have tested this demo based TWR-K60N512 with TWR-SER, and the Host is WIN7, but on my side it works well as expected. Please kindly refer to the following snapshot for more details.

Untitled.png

Untitled1.png

Untitled2.png


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信