K60 series DDR controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 series DDR controller

Jump to solution
2,171 Views
mneta
Contributor I

Hi all,

I am looking for a microcontroller in k60 series which supports ddr controller. I have looked in their K60 product brief where it says that they support DDR controllers but while choosing in the MCU solution advisor , k60 series doesnt feature ?? so I was wondering if anybody can tell me which microcontroller of K60 series supports DDR controller or it doesnt at all

 

Also does the tower system for K60 support  a USB host so as to put in a pen drive etc. , I am trying to figure this out yet.

Please reply

0 Kudos
Reply
1 Solution
1,900 Views
apanecatl
Senior Contributor II

Hi Nitesh, these are the K60 parts supporting a DDR interface:

  • MK61FX512VMJ12
  • MK61FN1M0VMJ12

The mini USB connector attached to the WTR-K60xxx boards can only be used to program/debug, however if you are using the complete kit you can attach your USB drive to the TWR-SER USB port.


View solution in original post

0 Kudos
Reply
1 Reply
1,901 Views
apanecatl
Senior Contributor II

Hi Nitesh, these are the K60 parts supporting a DDR interface:

  • MK61FX512VMJ12
  • MK61FN1M0VMJ12

The mini USB connector attached to the WTR-K60xxx boards can only be used to program/debug, however if you are using the complete kit you can attach your USB drive to the TWR-SER USB port.


0 Kudos
Reply