K60 series DDR controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K60 series DDR controller

跳至解决方案
2,184 次查看
mneta
Contributor I

Hi all,

I am looking for a microcontroller in k60 series which supports ddr controller. I have looked in their K60 product brief where it says that they support DDR controllers but while choosing in the MCU solution advisor , k60 series doesnt feature ?? so I was wondering if anybody can tell me which microcontroller of K60 series supports DDR controller or it doesnt at all

 

Also does the tower system for K60 support  a USB host so as to put in a pen drive etc. , I am trying to figure this out yet.

Please reply

0 项奖励
回复
1 解答
1,913 次查看
apanecatl
Senior Contributor II

Hi Nitesh, these are the K60 parts supporting a DDR interface:

  • MK61FX512VMJ12
  • MK61FN1M0VMJ12

The mini USB connector attached to the WTR-K60xxx boards can only be used to program/debug, however if you are using the complete kit you can attach your USB drive to the TWR-SER USB port.


在原帖中查看解决方案

0 项奖励
回复
1 回复
1,914 次查看
apanecatl
Senior Contributor II

Hi Nitesh, these are the K60 parts supporting a DDR interface:

  • MK61FX512VMJ12
  • MK61FN1M0VMJ12

The mini USB connector attached to the WTR-K60xxx boards can only be used to program/debug, however if you are using the complete kit you can attach your USB drive to the TWR-SER USB port.


0 项奖励
回复