K60 series DDR controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 series DDR controller

ソリューションへジャンプ
2,186件の閲覧回数
mneta
Contributor I

Hi all,

I am looking for a microcontroller in k60 series which supports ddr controller. I have looked in their K60 product brief where it says that they support DDR controllers but while choosing in the MCU solution advisor , k60 series doesnt feature ?? so I was wondering if anybody can tell me which microcontroller of K60 series supports DDR controller or it doesnt at all

 

Also does the tower system for K60 support  a USB host so as to put in a pen drive etc. , I am trying to figure this out yet.

Please reply

0 件の賞賛
返信
1 解決策
1,915件の閲覧回数
apanecatl
Senior Contributor II

Hi Nitesh, these are the K60 parts supporting a DDR interface:

  • MK61FX512VMJ12
  • MK61FN1M0VMJ12

The mini USB connector attached to the WTR-K60xxx boards can only be used to program/debug, however if you are using the complete kit you can attach your USB drive to the TWR-SER USB port.


元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,916件の閲覧回数
apanecatl
Senior Contributor II

Hi Nitesh, these are the K60 parts supporting a DDR interface:

  • MK61FX512VMJ12
  • MK61FN1M0VMJ12

The mini USB connector attached to the WTR-K60xxx boards can only be used to program/debug, however if you are using the complete kit you can attach your USB drive to the TWR-SER USB port.


0 件の賞賛
返信