K60 comparator input to output delay

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 comparator input to output delay

ソリューションへジャンプ
2,149件の閲覧回数
bhh
Contributor II

Is there a specification for the propagation delay of the K60 comparator input to output (continuous mode)?  The reference manual calls this Tpd, but I haven't been able to find an actual value.

0 件の賞賛
返信
1 解決策
2,081件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Brian,

You can find this value in the datasheet, just as the Fig 1 shows.

Please check the datasheet through the link as below by yourself.

http://cache.freescale.com/files/32bit/doc/data_sheet/K60P100M100SF2V2.pdf?fasp=1&WT_TYPE=Data%20She...

2015-04-07_15-30-21.jpg
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,081件の閲覧回数
bhh
Contributor II

I must have overlooked it before.  Thanks!

0 件の賞賛
返信
2,082件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Brian,

You can find this value in the datasheet, just as the Fig 1 shows.

Please check the datasheet through the link as below by yourself.

http://cache.freescale.com/files/32bit/doc/data_sheet/K60P100M100SF2V2.pdf?fasp=1&WT_TYPE=Data%20She...

2015-04-07_15-30-21.jpg
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信