K60 UART interrupt is stuck

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K60 UART interrupt is stuck

1,823 次查看
gerry26
Contributor I

Hi,

My UART interface RX stream is stuck and no new RX interrupt  is received for any attempt to drive input.

I experience a UART overflow, caused by interrupt long latency, which leaves the system with no active interrupt but with a char in the buffer.

This prevents from new char to be received. the only thing that "releases" the UART interface is D read.

Following this read the interface is released and the RX flow runs once again.

The UART statuses doesn't apply to any reasonable cause.

See UART status log below:

4006A000: 00 36 00 2C C8 40 00 XX 00 00 08 00 00 00 00 AA

4006A010: 22 00 C5 00 00 01 00 AA 00 00 00 0A 00 01 00 00

4006A020: AA 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

4006A030: 00 00 AA AA AA AA AA AA AA AA

Please note that the XX located in 4006A007 is the D register. Once this address is called the block is released.

Tnx,

Gerry

标记 (3)
0 项奖励
回复
1 回复

1,298 次查看
mjbcswitzerland
Specialist V

Gerry

When an overrun takes place the overrun flag must be correctly cleared otherwise the UART receiver will not process further reception.

Please see the following with explanation of how to reset it (towards the end of the thread): Lost UART interrupt on MK60DN512xxx10

Regards

Mark

0 项奖励
回复