K60 SPI Chip Select Problem ? PCS(0) not asserted in DSPI0 module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 SPI Chip Select Problem ? PCS(0) not asserted in DSPI0 module

ソリューションへジャンプ
3,447件の閲覧回数
yanam
Contributor II

Hello


I am able to generate clock and data using the following code. However the chip-select is not triggered or asserted automatically. I believe I am missing something, can anyone point out.


Initialization Code:

SPISelectPtr = SPI0_BASE_PTR;

            // Turn on the clock

            SIM_SCGC6 |= SIM_SCGC6_DSPI0_MASK;

      

            // Select pins

            // Clock

            PORTC_PCR5 &= (~PORT_PCR_MUX_MASK);

            PORTC_PCR5 = PORT_PCR_MUX(2) | PORT_PCR_DSE_MASK | PORT_PCR_PE_MASK | PORT_PCR_PS_MASK;

            // Sout

            PORTC_PCR6 &= (~PORT_PCR_MUX_MASK);

            PORTC_PCR6 = PORT_PCR_MUX(2) | PORT_PCR_DSE_MASK | PORT_PCR_PE_MASK | PORT_PCR_PS_MASK;

            // Sin

            PORTC_PCR7 &= (~PORT_PCR_MUX_MASK);

            PORTC_PCR7 = PORT_PCR_MUX(2) | PORT_PCR_DSE_MASK | PORT_PCR_PE_MASK | PORT_PCR_PS_MASK;

      

            //Chip Select 0

            PORTD_PCR0 &= (~PORT_PCR_MUX_MASK);

            PORTD_PCR0 = PORT_PCR_MUX(2) | PORT_PCR_DSE_MASK | PORT_PCR_PE_MASK | PORT_PCR_PS_MASK;;

      

            PORTD_PCR4 &= (~PORT_PCR_MUX_MASK);

            PORTD_PCR4 = PORT_PCR_MUX(2) | PORT_PCR_DSE_MASK | PORT_PCR_PE_MASK | PORT_PCR_PS_MASK;;

    // Select Master Mode

    // Continous Clock is disabled

    // FRZ is disabled, can be enabled later using SPI_MCR_FRZ_MASK

    SPI_MCR_REG(SPISelectPtr) = (SPI_MCR_DCONF(0) | SPI_MCR_MSTR_MASK | SPI_MCR_PCSIS(0) | SPI_MCR_PCSIS(1) | SPI_MCR_PCSIS(2)

                                | SPI_MCR_CLR_TXF_MASK | SPI_MCR_CLR_RXF_MASK);

    // Frame Size = 8

    // CPOL = 1

    // CPHA = 1

    // Delay after Transfer Prescaler value is 5

    // Baud Rate Prescaler value is 1

    SPI_CTAR_REG(SPISelectPtr, 0) = SPI_CTAR_FMSZ(8) | SPI_CTAR_CPOL_MASK | SPI_CTAR_CPHA_MASK | SPI_CTAR_PDT(2) | SPI_CTAR_BR(6);

Test Function to call byte write

void vTestWriteByteToSPI(uint8_t u8Data, uint8_t chip_select)

{

    SPI_MemMapPtr SPISelectPtr = SPI0_BASE_PTR;

    // Making sure no chip select beyond 0 and 1

    chip_select &= 1;

    // Write a byte with CS0

    SPI_PUSHR_REG(SPISelectPtr) = SPI_PUSHR_TXDATA(u8Data) | SPI_PUSHR_CONT_MASK | SPI_PUSHR_CTAS(0) | SPI_PUSHR_PCS(chip_select + 1);

    // Wait Until Read Flag

    while (!( SPI_SR_REG(SPISelectPtr) & SPI_SR_RFDF_MASK ));

    // Clear Read Flag

    SPI_SR_REG(SPISelectPtr) |= SPI_SR_RFDF_MASK;

}

I am using Freescale ARM Compiler, CodeWarrior 10.4. There are pull ups on the board for CS pins. Please help pointing out mistake if any.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,394件の閲覧回数
yanam
Contributor II

The SPI_PUSHR_CONT_MASK was a problem. After removing it from OR switches, chip select is working perfect. I have improved the code now, if anybodys interested, will post it.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,395件の閲覧回数
yanam
Contributor II

The SPI_PUSHR_CONT_MASK was a problem. After removing it from OR switches, chip select is working perfect. I have improved the code now, if anybodys interested, will post it.

0 件の賞賛
返信
2,394件の閲覧回数
prajnithkumar
Contributor I

Hi Yogenda,

It will be really helpful if you could post the improved code which you have mentioned, I'm beginner on Kinetis development and having hard time finding SPI driver.

Thanks in Advance

0 件の賞賛
返信