Anyone built USB DFU example for KL25?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Anyone built USB DFU example for KL25?

1,585件の閲覧回数
frankvanhooft
Contributor III

Just curious if anyone has managed to build the USB DFU example project for the KL25 processor?

I've tried building it from the latest (v 4.1.1) USB stack code, using CodeWarrior 10.4  I got a whole bunch of warnings / errors. I contacted Freescale tech support, who confirmed / replicated the problem. But I know there are some smart people on these forums, and I wondered if anyone else came across this same problem and then found a solution.

Thanks.

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 返信

1,310件の閲覧回数
antonioconcio
NXP Employee
NXP Employee

Hi Frank,

Is your CW up-to-date? I mean if the MCU 10.4 Processor Expert Update 1.0.1 update has been done.

Regards,

Antonio